2025-02-20 6:04 AM - edited 2025-02-20 11:16 AM
Hi everyone,
I'm working with the NUCLEO-U575ZI-Q board and using the ADC_SingleConversion_TriggerSW_Init example. However, I can't get the ADC to measure correctly. No matter what voltage I apply to pin 9 of CN7, the reading always stays around 80mV.
STM32 Version: 1.17.0
Has anyone encountered this issue before? Could I be missing something in the configuration?
Thanks in advance!
2025-02-20 6:34 AM
The NUCLEO-L575ZI-Q board doesn't have a ADC_SingleConversion_TriggerSW_Init example, either in GitHub or CubeMX. Show the code you're using, it could be any number of things. Are you using the correct pin and channel? pin 9 on CN7 is PA4.
Set the pin as a GPIO output and toggle it, can you see the voltage change on a multimeter?
2025-02-20 11:21 AM
Thank you for your quick response.
I made a mistake when mentioning the development board; I meant to say the STM32U575ZI-Q. I have already corrected it in the original post.
Sorry for the inconvenience.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.