2015-10-19 1:38 AM
Hi,
I would like to make sure that an active low signal is inactive when I call GPIO_Init(). My first idea is to set the ODR register via BRR/BSRR, i.e. with the GPIO_WriteBit() call before I call GPIO_Init(). Will that work or do I have to set the ODR register directly. Beyond that, what is the proper way of dealing with the active low situation. I hope you can help, Kilian2015-10-21 12:29 AM
Hi,
I tried using the GPIO_WriteBit() call before GPIO_Init() and it works as hoped for. Regards, KilianWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.