2020-09-12 1:28 PM
Hi
When I configure uart in interrupt mode, can I use it in polling mode in the future? (For any reason)
my other question, when is the HAL_UART_RxCpltCallback function called, is it when all data is received ? or when byte by byte is received?
Thank you
2020-09-12 2:04 PM
You can configured UART in interrupt or polling mode at will, but it can't really be in both modes at the same time. And if you have it in interrupt mode, you will need to stop it before using it in polling mode.
In interrupt or DMA mode, HAL_UART_RxCpltCallback is called when all bytes are received.
2020-09-12 2:22 PM
Thanks for yore reply
(you will need to stop it before using it in polling mode) well,how stop it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.