2025-11-10 12:36 PM
Hello ST Community team,
On the DS11532:
Could you please have a look.
Best Regards.
II
Solved! Go to Solution.
2025-11-10 1:52 PM - edited 2025-11-11 12:36 PM
Hi @Issamos ,
There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.
I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).
Thank you for your contributions.
(PS: Internal ticket number 221536 is not accessible or usable by customers).
2025-11-10 12:41 PM
Hello @Issamos ,
Thank you for having reported this.
I will check this and come-back to you soon with updates.
2025-11-10 1:52 PM - edited 2025-11-11 12:36 PM
Hi @Issamos ,
There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.
I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).
Thank you for your contributions.
(PS: Internal ticket number 221536 is not accessible or usable by customers).
2025-11-14 5:14 AM
Hi @Issamos ,
After deep check, we have concluded that the STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.
So, the following sentence in DS11532 under Figure 1 (page 19) :
"The STM32F76x LQFP144, LQFP176, LQFP208, TFBGA216, UFBGA176 packages are fully pin to pin compatible with STM32F4xx devices."
will be changed to:
“The STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.”
For further details, I recommend consulting AN4660, section 1.1.4 “TFBGA216 package,” which provides a through explanation of this compatibility.
Thank you for your contribution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.