2020-04-02 10:17 AM
I have nucleo-64 STM32L476 board. I have initialised ADC. I am able to read all the three channels ( that I configured in cube Mx) correctly using DMA.
Then I added SD interface. I was able to read and write in the SD Card as well. But as soon as I initialise SD card, my ADC readings gets distorted ( not correct).
SO I traced at which point of SD intialisation this happens and found that as soon as
/* Enable SDMMC Clock */ ( in file STM32L4xx_hal_sd.c and function HAL_StatusTypeDef HAL_SD_InitCard(SD_HandleTypeDef *hsd) )
__HAL_SD_ENABLE(hsd); is executed, the ADC reading gets distorted.
SO commented this line, for testing purpose and found that ADC reads correctly.
Now clock configuration is that ADC CLk is at 12 Mhz and SDMMC Clk = 48 Mhz
both derived from PLLSAI1
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_USART2
|RCC_PERIPHCLK_SDMMC1|RCC_PERIPHCLK_ADC;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_PLLSAI1;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_PLLSAI1;
PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSE;
PeriphClkInit.PLLSAI1.PLLSAI1M = 1;
PeriphClkInit.PLLSAI1.PLLSAI1N = 12;
PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV7;
PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV2;
PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV8;
PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK|RCC_PLLSAI1_ADC1CLK;
can any body help to sort this problem.
Thanks in advance.
Thanks
Hitesh
2020-04-02 8:40 PM
Did you check the errata sheet?
Did you check schematic to ensure pins are separated?
2020-04-02 11:38 PM
Thanks for the reply.
I have gone through the errata sheet for my device and did not found such problem.
Also as far as pins are concerned, they are quit different
for ADC using lines: PC0,PC1 & PC2 while for
SD using pins PC8, PC9, PC10,PC11,PC12 & PD2
Thanks,
Hitesh
2020-04-02 11:47 PM
HI ..
with respect to the above problem, would like to share some more details,
The sequence followed
/* Initialize SDMMC peripheral interface with default configuration */
status = SDMMC_Init(hsd->Instance, Init);
__HAL_SD_DISABLE(hsd); /* Disable SDMMC Clock */
status = SDMMC_PowerState_ON(hsd->Instance);
__HAL_SD_ENABLE(hsd);
2020-04-02 11:47 PM
HI ..
with respect to the above problem, would like to share some more details,
The sequence followed
/* Initialize SDMMC peripheral interface with default configuration */
status = SDMMC_Init(hsd->Instance, Init);
__HAL_SD_DISABLE(hsd); /* Disable SDMMC Clock */
status = SDMMC_PowerState_ON(hsd->Instance);
__HAL_SD_ENABLE(hsd);
2020-04-02 11:50 PM
HI ..
with respect to the above problem, would like to share some more details,
The sequence followed
/* Initialize SDMMC peripheral interface with default configuration */
status = SDMMC_Init(hsd->Instance, Init);
__HAL_SD_DISABLE(hsd); /* Disable SDMMC Clock */
status = SDMMC_PowerState_ON(hsd->Instance); // there is 2 ms delay in this fuction
__HAL_SD_ENABLE(hsd); /* Enable SDMMC Clock */
Enabling SDMMC clock distorts the ADC readings.
2020-04-03 6:54 AM
> my ADC readings gets distorted ( not correct).
Consider better describing what you mean here. "Distorted" and "not correct" are not descriptive.
2020-04-03 7:27 AM
I have applied
CH1: 3.3 V
CH1: 1.27V
CH:3: 0V
This are read correctly as applied without __HAL_SD_ENABLE(hsd); /* Enable SDMMC Clock */
once SDMMC Clock is enabled it reads
CH1: 2.65V to 2.85V
CH2: 1.16 to 1.18
CH3: 0.002V
Thanks,
Hitesh
2020-04-03 7:35 AM
Thank you, that is a much better description. Can you max out your sample time and see if readings improve? If that doesn't work, I can't really think of anything else it may be.
2020-04-03 7:46 AM
Sampling time is already maximum.
Thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.