2010-07-15 8:22 AM
A warning about parity mode on the UART
2011-05-17 4:58 AM
Table 179 in revision 10 of the reference manual seems to be quite clear.
Did you see this table?2011-05-17 4:58 AM
Nope, mine is revision nine and table 179 doesn't mention it.
2011-05-17 4:58 AM
In revision 9, it is table 177.
In revision 1, it is table 68.2011-05-17 4:59 AM
This should be referenced from the register descriptions and I still think it's poorly worded (like much of ST's documentation, sadly).
2011-05-17 4:59 AM
This is something that could be handled by ST's Standard Peripheral Library USART module but isn't (in v3.3.0).
2011-05-17 4:59 AM
thanks robert. i just read it before using nine bit protocol :)
and also agreed about the bad documentation of ST :( except firmware library user manual which is quite better
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.