2021-04-23 12:06 AM
Hi. I realize this may seem simple to some of you but i realy want to undestand this as easy as it is possible.
In STM32 (for example) there is a bit called STKALIGN. If this bit is set stack is align to 8 byte instead of 4 byte.
How can i see difference in behavior when this bit is set or not? How to use this?
I know wthat align is but it is hard to undestand if i do not see how it works.
2021-04-23 1:43 AM
See here to understand why it is needed:
How it works:
Assume that interrupt strikes just after the program pushed a word on the stack, so the stack is not 8 bytes aligned.
To align the stack for the handler, hardware automatically pushes one more word as part of "stacking" procedure, and sets bit 9 of the saved PSR to remember this.
On exit from the handler the stack is automatically restored.
The fine manual to read is PM0253. Enjoy ))
--pa
2021-04-25 9:23 PM
Hi.
I read this couple of times trying to understand this. But that raised even more questions :)
How can i see this is needed?
How can i see this work?
2021-04-26 12:15 AM
Hmm... perhaps read it another time?
2021-04-27 1:27 AM
Probably this will be hard to obserwe. But when stack isn't 8byte aligned and in interrupt some 64-bit variable will be allocated on stack, then will be a problem. but chance for this is low and effect is unpredicted.
2021-04-27 3:51 AM
This is trivial to observe: 1.when SP is aligned on 8, push a word. Now SP is not aligned on 8. 2. Cause an interrupt, SVC for example
--pa
2021-04-27 4:07 AM
forcing this without any efects isn't an observation.
2021-04-27 10:25 AM
So Pavel i took yours clever advice, I've looked there one more time andto my surprise nothing more appeared. No more example explaining how it works. What is benefit of this 8 byte align. How can i use it.
2021-04-27 11:43 AM
The Cortex-M parts people are discussing here don't have the 64-bit data paths that would be an issue for LDRD/STRD and LDM/STM against 32-bit aligned addresses.
I don't recall VPUSH/VPOP being an issue.
Alignment and data access The following data accesses always generate an alignment fault:
• Non halfword-aligned LDREXH and STREXH
• Non word-aligned LDREX and STREX
• Non word-aligned LDRD, LDMIA, LDMDB, POP, LDC, VLDR, VLDM, and VPOP
• Non word-aligned STRD, STMIA, STMDB, PUSH, STC, VSTR, VSTM, and VPUSH
2021-04-27 11:46 AM
It is for architectures where the data paths, busing, or memory subsystem have 64-bit paths, and where additional time penalties will occur when transactions are split.
The ABI recommendation is for cross-platform harmony and ease of porting.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.