2023-10-02 5:51 AM
Hello team,
We are looking to generate a sine function of 50 Hz frequency using the STM Cordic.
Can you please share the theta range in this case. While we are giving 0 to 1 or 0 to 2pi (normal theta range), the resulting sine wave is not as per expectation. Please share a code for our reference.
Also, if we want to use the Matlab embedded libraries, what should be the data type and conversion expected in this case?
Requesting your earliest inputs!
Thank you!
Best Regards,
Madhura
2023-10-02 6:06 AM
I've never used this but I found this link...
https://www.st.com/resource/en/product_training/STM32G4-Peripheral-Cordic_Coprocessor_CORDIC.pdf
Suggests that the cordic input is normalised by pi radians in the -pi to +pi range, which equals -1 to 1.
As described in the document these input values are signed fixed point, so the numeric range is therefore -1 (0x80000000) to 1 - (2^31) (0x7FFFFFFF).
Hope this helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.