2020-04-02 10:39 AM
Hello,
When trying to use ADC, I ran into a problem that I don't really understand.
If I try to use ADC through the PA4 pin, the values read fine and are correct.
However, when I try to use any of the other pins for ADC, none of them seem to read the correct values.
Any help / explanation as to why this may be happening would be appreciated.
Thank you.
Edit:
I've also tried the code on two other 32L04538Discovery boards and the same problem persists. PA4 works fine for ADC, but none of the other pins do.
2020-04-02 11:50 AM
Are the pins you've tried disconnected from the on-board circuitry of the 'L053DISCO board?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.