2017-06-14 9:04 AM
I have a 32F412GDISCOVERY (the one with LDC) board and the stock demonstration firmware is nowhere to be found. I can find the firmware to other discovery boards, but not this one. How can I obtain this firmware source code package?
2017-06-16 4:42 PM
Just pulled Cube F4 v1.16, and built with Keil uV5.22
Doesn't have a Flash Algorithm for the SPI NOR Flash at 0x90000000, so used the ST-LINK Utilities to burn instead of Keil, but seems to run without faulting.
2017-06-17 2:07 PM
Now migrated the current FatFs release supporting FATX, will need to benchmark with some 64 or 128GB cards
2017-06-17 2:09 PM
Just been through the F412G-DISCO code and there is some awfully broken DWT->CYCCNT code in there. HAL_GetTick() doesn't wrap properly in the 32-bit number space.
2017-06-17 2:17 PM
Probably a wise move, better you build your apps the way you are comfortable with, and strip out the pieces you need from demo/example code as you need to, rather than try and add stuff into code built with a different mindset.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.