2024-04-13 4:12 AM - edited 2024-04-13 4:16 AM
Hello all,
I am trying to interface 24C16RP EEPROM with my MCU soldered on breakout board and it seems like the EEPROM is behaving very weird when i am trying to write and read. first of all it starts to write from position 1 not from zero of an array that i have created to store the data and i tried a lot to figure out the cause but i couldn't and the weird part is that after writing to a specific page if am trying to read any other page of the entire page address it returns the same date i have written to it. As i know this EEPROM has 16 byte of page size and 128 pages correct me if i am wrong. With that said i am attaching the cube mx code and the ioc file and some screen short for your better understanding. Please help me if you find something error in my code.
Thanks
uint8_t data_Read[16];
uint8_t data_Write[16]="1234567898765432";
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART1_UART_Init();
HAL_I2C_Mem_Write(&hi2c1, 0XA0, 1, 2, data_Write, 16, 1000);
HAL_Delay(5);
HAL_I2C_Mem_Read(&hi2c1, 0XA0, 9, 2, data_Read, 16, 1000);
while (1)
{
HAL_UART_Transmit(&huart1, data_Read, 16, 1000);
HAL_Delay(1000);
}
}
2024-04-15 1:22 AM
If You set MemAddress to 6 You will read starting from Byte 6 (so probably what You read is "James...!!") if You want to access the 6. 16Byte page you have to set MemAddress to 16*6 = 96.
2024-04-15 1:55 AM - edited 2024-04-15 1:59 AM
uint8_t data_Read[16];
uint8_t data_Write[16]="hello james...!!";
So, i can only write with the gap of 16,
means page 1 = 16byte = index 0 to 15
page 2 = 16byte = index 16 to 31
page 3 = 16byte = index 32 to 47 and so on...
And for reading page 1's entire content i have to put
HAL_I2C_Mem_Read(&hi2c1, 0xA0, 1, 1, data_Read, 16, 100);
it will return me the entire 16byte of the content and if i use any number below 16byte it will return me the data from where i have requested like
HAL_I2C_Mem_Read(&hi2c1, 0xA0, 3, 1, data_Read, 16, 100);
it will return page 1's llo james...!! from page 1 and and 3bytes of data from page 2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.