2022-03-02 7:07 PM
2022-03-14 7:45 AM
Hello @SLee.8 ,
I will answer in english if you don't mind ;-). Yes the datasheet STM32H723 Tables 54 or 55 (respectively HSLV = OFF or ON) the limit in frequency of the IO ports depending of the load C.
Speed=11 select the maximum speed (maximum consumption).
The max operating frequency of the PWM though the timers is in "6.3.35 Timer characteristics" (details by timers in 3.31 Timers and watchdogs)
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.