2015-08-26 12:19 AM
Hi,
i want to run motors with Rs < 0.01 Ohm and Ld<0.010 mH (low voltage high current), but the Motor Control Workbench is limited to this values. Can someone give me the formula to compute all the parameters from the header files, to do it by myself? Thanks for your help Marco #motor-control-workbench2015-09-07 5:36 AM
Ciao Marco
It is an information that we can't deliver in this way. I suggest to contact you nearest ST sales office. Ciao Gigi2021-06-27 9:01 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.