2021-10-05 9:00 AM
Hello,
I purchased X-NUCLEO-IHM15A1 DC Brush motor controller, which is supported by BSP X-CUBE-SPN15. Documentation specifies three supported Nucleo-64 boards; I purchased NUCLEO-STM32F401RE.
How to find the F401RE .ioc file to enable resources needed by IHM15A1?
Thank you.
2021-10-12 8:42 AM
Apparently the SPN15 software was developed before MX .ioc files where created? Thus no .ioc file?
IHM15A1 mostly works, but still have not determined why Motor B will not run backward with the demo software in DUAL mode. Have replaced both the F401RE MCU and the IHM15A1Motor Driver board. Have also swapped the motors between Channel A & Channel B. The IHM15A!/SPN15 software does not drive Motor B during demo steps 1-4 with the hardware jumper set to DUAL. It all works fine in PARALLEL,
It seems likely that there may be a defect with the particular IHM15A1 expansion boards that I purchased, because it looks like the SPN15 software works just fine.
2022-11-29 6:50 AM
An *.ioc file for the X-NUCLEO-IHM15A1 would be very helpful.
Now I have to transfer the old SPN15 world to the new *.ioc world. I will use the X-NUCLEO-IHM15A1 together with the NUCLEO-F091RC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.