2018-12-02 7:32 AM
As far as I know, to use the application in torque control mode. I will have to set it to control m
ode in ST workbench which is in drive setting on the upper right box. and in firmware I will just add in MC api which is MC_ProgramTorqueRampMotor1() with final torque value and time taken to ramp the value. But I have a question due to I have not much of understanding of motor torque . What is the value to be put in torque value? current value , or actual torque value? and will the equation of converting sampled from ADC or PWM will be similar to speedramp equation? Thanks
2021-06-22 2:07 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.