2024-05-10 1:59 AM
Hello community members,
I'm currently in the final stages of preparing a prototype, and I've encountered a problem with motor synchronization.
Here's the setup: I'm utilizing the EVspinG4-Dual Board to control two brushless motors (hoverMotors), which have been profiled using X-NUCLEO-IHM08M1. After profiling, I developed a project using MotorControl Workbench 6.2.1.
The issue I'm facing is that upon testing, I noticed a discrepancy in the response times of the motors. Motor 1, connected to the STSPIN32G431, is experiencing a delay in reaching the target speed, while motor 2, connected to the STDRIVE101, achieves the target speed immediately. Despite configuring both motors with a ramp speed and a delay of 0, motor 1 consistently ramps slower compared to motor 2.
I appreciate any insights or assistance you can provide in resolving this synchronization issue. Thank you for your attention to this matter, and I look forward to any suggestions you may have.
2024-05-17 1:44 AM
Hello @alila619,
Some issue around EVspinG4-Dual Board been fixed in our new MCSDK 6.3.0 release.
Could you please download it and try if it solved your issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.