2020-07-10 7:03 AM
Hello,
I'm working with NUCLEO F302R8 + X-NUCLEO IHM08M1.
I was wondering if it was possible to stop the motor in a fixed time with the Motor Control SDK library v5.4.4.
Thanks for the support,
2021-06-14 11:30 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.