2021-01-20 11:03 AM
We are working on parameter tuning for a BLDC motor on a custom board, by using demo board STEVAL-SPIN3201 and Motor Control Workbench (FOC mode). The motor is used to drive a peristaltic pump.
The motor has been measured and measurements have been verified (number of poles, back emf, inductance in both axis [this measurement is hard to perform with tight tolerance], hall sequence, etc...). However, we found that the suggested P and I values for speed regulator are generating high instability (the motor keeps vibrating for more than half the speed range), and we had to change them completely to get consistent results. Still, we are unable to run the motor at low speeds (i.e. below 100 mechanical RPMs). The torque ramp is always smooth (and no load speeds are smooth in torque mode, it looks like the current regulator is working correctly).
We identified the following motor parameters:
Some additional details:
Since tuning has proven to be so difficult, we are asking for suggestions here.
2021-03-01 2:00 AM
Dear @LF.1
Many thanks for your detailed question.
I forward it internally.
Best regards
==
Laurent Ca...
2021-11-30 12:32 AM
What are the suggestions for this issue? Was it solved and if yes, could the solution be provided to the community?
Best regards
Chris K.
2021-11-30 1:07 AM
Hello Chris,
unfortunately I got no word from ST. I suppose the parameter computation may be somehow broken in the software version I used and with the operating conditions of motors I had on hand. They seem to be aware of the limitations of their tools (and maybe they are working on that), but information is spread across a number of sources (videos, whitepapers, tool documentation, release notes...). In any case, closed loop stability with motors and FOC algorithms is not trivial.
The values we tweaked do not give fully satisfying results at low speed and high torque (instability, noise and slow torque reaction even on demo board). In addition, the resources of the microcontroller (program memory, RAM, speed and core) are very limited (not building without optimization, sometimes measurements are not fast enough) and there is very limited room to make changes. That's why we are planning to test both MCSDK 6 (to be due in the next months) and maybe STSPIN32G4, or a combination of a standard microcontroller and an external motor driver.
The day where ST will finally understand that software quality, support and documentation has the same importance of (their very good) hardware products perhaps their will outsell their competitors...
Best regards,
Fabrizio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.