2012-01-05 8:55 PM
2012-01-09 12:11 AM
The STM32 FOC PMSM SDK OverCurrent protection acts like an emergency stop. In particular it is performed exploiting the feature of the PWM timer that disables (putting in a predefined state) the six outputs. These signals are kept disabled until the user send another start motor command (after the faut acknowledge).
Regards Gigi2021-06-21 9:38 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.