2024-10-04 3:06 AM
Hello,
I am using MCSDK_v6.3.1 and encountered a problem when changing TIM1 PWM pins:
When I now want to create a project with the modified inverter, I get this error:
Error
It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory features:
- Phase Voltage Generation
For more details, please, look at the following log file in your home directory: .st_workbench/connectAlgo.log
Solved! Go to Solution.
2024-10-04 3:16 AM
2024-10-04 3:16 AM
Solved. I mixed up PC0 and PC2.
Thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.