2014-10-06 9:57 AM
I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration are incorrect, it has 4.0 .net installed also.
2014-10-16 10:46 AM
This forum is where messages go to die
2014-10-16 11:55 PM
Ciao
Mybe you can have better luck there:https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards
There are covered dSpin products Ciao Gigi2021-06-17 1:30 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.