2015-08-20 2:00 AM
Hi all,
I'm using Rowley Crossword IDE for MacOS and i have issue with compiling WEB FOC v4.1.0 project (import from Keil uVision project). Always when i try to build project i get this error: ''Can't open /PROJECT ADDRESS/BUILD CONFIGURATION/tmpdFtZGh for reading''. I used FOC v4.0 in Rowley CW and everything is OK. I checked access rights and seem's to be OK.Do you have any idea to solution? Thanks for your help and time Ondra2015-08-21 3:00 AM
I downloaded foc support file from link given below but it is not even opening.
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257936?icmp=pf257936_pron_pr_jan2015&sc=stsw-stm32100-pr2015-09-07 5:39 AM
Hi
I'm sorry We deliver the FW package with the support only for IAR and KEIL and we can't provide any help for other IDEs. Regards Gigi2015-09-07 5:43 AM
Ciao
Seems that now the link is working. Anyhow I suggest don't trust in hyperlink and prefer to search in the ST.com the P/N of the library that will be allways: STSW-STM32100 Ciao Gigi2021-06-27 10:54 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.