2018-07-15 12:29 PM
I have the NUCLEO-IHM07M1 motor dev board along with the NUCLEO-F302R8 mcu dev board. I've tried to get the demo software working with the ST Motor Control Workbench but am getting a Speed Feedback fault each time I try and start the motor. I'm able to connect to the dev board in the workbench, see the correct bus voltage, etc. But as soon as I start the motor, the rpm gauge goes all over the place for a bit before reporting the fault. Almost as if there are floating inputs to hall sensors or something. I've read through as much documentation as I can find and I am reasonably confident I have the sw and jumpers configured correctly for FOC control. Any ideas what could be causing this fault?
Thanks
2021-06-22 2:20 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.