2020-04-03 3:25 AM
2020-10-15 10:25 AM
Dear Laurent,
The problem was in the USB cable that transmitted power but no data.
I changed the cable and it is working now.
Btw, it would be a good idea to provide the cable with the board!
Best regards,
Mohamad
2020-04-03 5:21 AM
Hello MKOTE.1,
Can you please specify which SW you are using?
Thanks and best regards,
Claire
2020-04-03 9:54 AM
Hello Claire,
I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.
This is the first time I use the board, I've never seen the LED LD2 blinking.
Thanks,
Mohamad
2020-04-09 12:59 PM
Hello Claire,
I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.
This is the first time I use the board, I've never seen the LED LD2 blinking.
Thanks,
Mohamad
2020-04-15 9:48 AM
Any other suggestions? I need to be able to program the board.
2020-10-15 2:43 AM
Dear @MKOTE.1
Do you have still this problem to solve?
If not, do not hesitate to share the final solution you found.
Best regards
Laurent Ca...
2020-10-15 10:25 AM
Dear Laurent,
The problem was in the USB cable that transmitted power but no data.
I changed the cable and it is working now.
Btw, it would be a good idea to provide the cable with the board!
Best regards,
Mohamad
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.