2021-07-09 9:40 AM
when used custom board how to used motor profiler for detect motor parameter
motor parameter calculated in stm32 or in motor control profiler
2021-07-09 9:43 AM
Hello,
For the time being, the motor profiler can be used only on the ST boards proposed by the tool.
Regards
Cedric
2021-07-09 9:50 AM
calculated motor parameter in stm32 ic or in side motor control profiler
2021-07-09 9:58 AM
The motor parameters are computed by the MCU with a dedicated firmware. This firmware is generated for all proposed boards it is why it is not open yet to custom boards. The PC tool is not involved in the parameters detection.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.