2021-08-10 5:57 AM
Unfortunately, I do not have much info as to what causes this. I am using the FOC library with a 3-phase BLDC and encoder as speed feedback. Sometimes when I send a ramp command, the motor flies to ~5000 RPM regardless of the target speed I set. It is very infrequent. It can be fixed by cycling power it seems. Anyone run into similar issue?
2021-09-05 3:07 AM
Dear @nmamore
We need more data to help you (configurations, pictures, screenshots, etc.).
Is it possible?
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.