2020-03-25 7:45 PM
I have set the jumper pins with respect to the user manual.
The motor only runs after I profile it at the motor profiler, when I run the program into the board using the STM32CubeIDE, the motor stops running again. And when i want to profile it again it says that a firmware upgrade is needed for the board to connect to the profiler.
2021-06-27 9:38 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.