cancel
Showing results for 
Search instead for 
Did you mean: 

I am using X-NUCLEO-IHM08M1 NUCLEO-F446RE Motor Profiler 5.4.8 motor>>48v 600w not run

somkid
Associate III

0693W00000Un8ovQAB.pngI want you to help explain and help fix it.0693W00000Un8pUQAR.pngMotor 48 volts, 600 watts, number of pairs of poles 52/2=26

or the motor is too big, please reply, thank you very much.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

I ran into that problem.Troubleshooting is very difficult.Doesn't work as intended

I tried to fault-find the circuit but it is almost impossible without any of the original design information. I ended up having to run my motor at 12V only during development then I will move to a custom board for the final product.

your work is interesting

Is there a project that will be used with a motor of any size? 48v 72v 84v

500w 1000w 2000w 3000w?

Can you share your experience?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.