2020-06-30 8:53 PM
i got a STEVAL-CTM010V1 board and installed the SDK(5.4.4 full),after that i created a project base on example(STEVAL-CTM010V1 dual drive with PFC,see pic_1),but the example does not enable the PFC feature(see pic_2),so if we want to use the PFC feature on CTM010V1 board ,what should we do ?
2020-07-01 12:20 AM
@Claire OKU (ST Employee)
2020-07-01 5:48 PM
i found a tips to fix this issue,just need to modify the config.xml file(C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.4\Utilities\PC_Software\STMCWB\assets\xml).
hence,if you remove the warning ,you can config the PFC feature on WB.
.
2021-06-15 12:42 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2022-08-30 5:43 AM
2023-11-16 3:00 PM
Any solution to this ?
many thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.