2024-11-05 2:27 AM
In motor control workbench 6 there is only HSO (which I don't understand if it's equal to HFI)
In motor control workbench 5 there is the option "sensorless + HFI" but it is not settable because it says "not supported in FW for SDK5.x"
Is there by any chance a version of motor control workbench that supports HFI + Sensorless ??
Thanks
Solved! Go to Solution.
2024-11-05 5:23 AM
Hello @luke514,
As mentioned in workbench tool, "sensorless + HFI" is not supported in FW for SDK5.x and following deliveries.
You can find a full HSO feature (that do not replace HFI feature) description in documentation available through "Workbench tool">About>Documentations>Documentation", "HSO Startup Guide" link.
2024-11-05 5:23 AM
Hello @luke514,
As mentioned in workbench tool, "sensorless + HFI" is not supported in FW for SDK5.x and following deliveries.
You can find a full HSO feature (that do not replace HFI feature) description in documentation available through "Workbench tool">About>Documentations>Documentation", "HSO Startup Guide" link.
2024-11-05 5:37 AM
Thank you for your response.
Where can I find your information/examples/implementations of the High Frequency Injection technique? ..since it is not present in MC Workbench
2024-11-05 5:52 AM
Let me explain better: since I cannot enable the HFI motor control workbench 5 option and since it does not exist in motor control workbench 6 ... do you have any libraries/guides to help me implement that technique?
In the mc_interface.c generated by motor control workbench I found only the function MCI_GetIqdHF, which I think it does not center with this :\
2024-11-05 7:58 AM
Hello @luke514,
As already mentioned, HFI is no longer available on Motor Control Workbench, as an example or in documentation.
MCI_GetIqdHF will be removed in the next versions as it is unused.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.