cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I want to use a STM32G474CBU with two motors, but I have the problem that I can't select "shared resources for both motors" in "Control Stage - Analog input and Protection". I am using MCSDK_v5.4.3.

UHerd.1
Associate

If I select a SM32F303CB I can select "shared resources for both motors" using ADC1/2 for both motors. I don't understand why it works for the STM32F303CB and not for the STM32G474CBU.

Because of space and simple layout I want to use a STM32 in a UFQFPN48 case for two motors and 3-shunt measurement and Encoders.

It would be nice if someone can give me answer to my problem.

Best Regards,

Ulf

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

Adding of the "SM32 Motor Control" topic.

Best regards.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.