2016-11-09 7:41 AM
Hello everyone.
Recently I started to create a project to make control of a BLDC engine.I used, until now, the compiler eclipse AC6. I have read here, in the forum, that some people are using the SDK with AC6.Can someone explain the procedure, please?Thank you very much. #ac6 #foc-sdk2017-01-10 12:53 AM
Hello
Martins.David
,You can refer to openSTM32 website.
Following link details how to install eclipse plugins to be able to compile CubeMX generated code:
http://www.openstmorg/Installing+System+Workbench+for+STM32+from+Eclipse?structure=Documentation
hope it answer your question.
If I missunderstood it, could you please elaborate a bit what you are trying to achive ?
Thanks in advance.
KR
Sirma
2021-06-15 4:36 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.