2021-08-26 10:42 PM
hi st community,
I am using NUCLEO-G431RB control board and STEVAL-IPM20B power board, generate the code using st-workbench. the board is connected with 1kw PMSM motor of 3000rpm.
Motor run fine up to 1200 rpm but rpm not increase after that, at that point the motor output power showing 200 W on monitor dial.
st work bench monitor screen has power dial of maximum 200W, is that limit or what? the power board capacity 2000W.
how can I achieve the full RPM with increase in output power.
thanks,
2021-08-30 3:44 AM
Hello,
From the top of my head, the parameters that can limit the speed of your motor are :
A percentage less than 95% will limit the maximum speed.
The 200W is a monitor limitation, not a real constraint.
Regards
Cedric
2021-09-01 2:32 AM
thanks cedric for reply,
the maximum RPM increase from 900 to 1050 then there is no further increased.
what are the other cause for limitation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.