2026-01-27 4:29 AM - last edited on 2026-01-27 5:20 AM by Peter BENSCH
Hello,
I want to drive a BLDC motor using the EVAL-L9907 in combination with the Nucleo-401RB board, and I want to use the STM32 Motor Control Workbench.
I have tried to configure a custom board for the EVAL-L9907 in the Motor Control Workbench, but I cannot set some of the functionality (e.g. current sensing, enable GPIOs).
Is there a way to obtain a JSON file for the EVAL-L9907 that I can import into the Motor Control Workbench?
Many thanks in advance.
2026-01-27 9:09 AM
Hello @Mechatronik,
The NUCLEO-F401RE board is available in Motor Control Workbench.
Use the STMC Board Designer tool to create a description file for the EVAL-L9907 board.
The tool is located in the ...\MC_SDK_x.x.x\Utilities\PC_Software\STMCBD directory.
Documentation is available in STMC Board Designer tool > About.
On the MCSDK firmware side, FOC current sensing supports single-shunt and three-shunt topologies. The L9907 gate driver is not supported.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.