2019-07-24 2:56 AM
i have generated code from motor control workbench and when i build this code the error came as,
region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ Problem
StSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_24_07 C/C++ Problem
i tried for optimised the code code then the there is no error but motor is not working well.......
2021-06-22 1:21 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.