2020-08-23 7:13 AM
Hi,
finally I bought an evalkit-robot-1 to try the stspin32f0 and start working with the Mcsdk.
I was able to compile the code on the st cube ide and program the controller with the stlink v3 and have the motor working using QModBus commands.
Now I want to make a step further by changing the control strategy and recompiling the code.
In particular I saw on another post that it is not possible change the control modality from position to speed or torque directly from the main but I need to change the control strategy in the workbench is it true?
I tried to do that but obiuvsly the code is now not working and the motor is not anymore initialising.
However, I don't know how to enable the debug with this system to see the variables or to printf some informations to debug the code.
Can you suggest the best procedure ?
Thank you in advance.
2020-09-14 2:12 AM
Dear GFont.2
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-20 8:27 AM
Dear @GFont.2
I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.