STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Motor control Workbench Monitor via serial

Posted on September 09, 2014 at 19:22I am trying to use the motor conrol foc library found in stsw-stm32003.  I am using an stm32f103 and am failing to understand the steps required to use the parameter files generated by the workbench so that I can...

justin2 by Associate
  • 2075 Views
  • 4 replies
  • 0 kudos

motor control in STM32 cortex M0

Posted on September 14, 2014 at 21:48Hi, would like to use STM 32 F0 for 3-phase motor control. Could anyone please let me know what evaluation board for motor control in STM32 F0 to purchase? ALso, I noticed that st’s library "STM32 PMSM FOC SDK ...

FOC 4.0 and STM32F4xx

Posted on September 18, 2014 at 21:34Hi, few days ago I downloaded the file ''STM32_FOC_SDK_4.0.0_Web_140625.exe'' from your homepage and wanted to try out the motion control on my custom board equiped with an STM32F407ZG device (either as single dr...

Problem with dspin

Posted on October 06, 2014 at 18:57 I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration...

sburr by Associate II
  • 1739 Views
  • 3 replies
  • 0 kudos

not stable at slow speeds PMSM FOC

Posted on October 30, 2014 at 15:31Hi I'm working with the motor from maxon: http://www.maxonmotor.ch/maxon/view/product/motor/ecmotor/ecmax/ecmax30/272768 When I drive the motor at slow speed (50rpm), the Speed is not stable because the resolution...

dominik by Senior
  • 2074 Views
  • 4 replies
  • 0 kudos

FOC SDK 4.2 clearing thumb mode with Eclipse AC6

Posted on January 03, 2016 at 15:27Hi,i recently ran into a problem with a FOC SDK 4.2 base motor control project.After assembling a project for Eclipse AC6 (API sources + EWARM library from web edition) I got usage faults during the execution of a ...

martin.k by Associate II
  • 1978 Views
  • 5 replies
  • 0 kudos

PMSM FOC SDK 4.0 code stucks

Posted on March 09, 2015 at 09:32Hello,I can't get PMSM library working. I don't have motor evaluation board, i have self-built board with STM32F303RB and i have F3 discovery. Problem is that program gets lost in library instructions and ends up stu...

firmware settings questions:

Posted on March 22, 2015 at 16:32Hi!I have 2 little problem:1:My Shunt value is  0.0005 ohm. Can i set it somehow in the motor firmware.The original lowest possible value is 0.001 ohm.2:I use 1 shunt settings, and STM32F303VC controller ic. This IC ...

kissmucus by Associate II
  • 1062 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.