2021-12-10 3:02 PM
Hello, does anyone know the correct procedure to tune the PI parameters for the ST FOC motor control solution?
My configuration:
Not that is should matter, but I am using a Nucleo 446RE controller with the STDRIVE101 eval board with 48V supply.
I am able to generate, build and load, I am using a BLDC with hall sensors. Everything works fine, I have some PI parameters where it runs ok.
In the Motor pilot I see PI parameters for Speed, Torque, and Flux. I am interested in speed control for my application.
I have noticed the altering the flux PI parameter and the speed PI parameters both effect the motor control.
My questions is what is the correct procedure for tuning the parameters, again I am only interested in speed control. Do I tune flux first then speed, other way around, both at the same time, just one and not the other, etc...?
Maybe someone know of an application note or youtube video that goes over this?
Thank you,
-Kyler
Solved! Go to Solution.
2021-12-12 11:30 AM
2021-12-12 11:30 AM
2021-12-13 1:31 PM
great thank you, this is what i was looking for.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.