2023-12-20 1:00 AM
Hi.., Currently, I'm using STSPIN32F0601 and driving the BLDC motor using ST-MCSDK-5.4.5 and I'm very new to it. After spending a couple of weeks studying, I know how to call the API to check parameters like VBUS, Motor Speed, Motor Power, Phase current, and so on. The problem that I'm facing is I would like to check the Duty Cycle of the PWM signal when the motor is running. So.., may I know how I can see the real-time duty cycle of the PWM.
Thanks for your reply and help.
2023-12-21 7:40 PM
I use MCSDK 6.2.0 the duty cycles are available in the function
__weak uint16_t PWMC_SetPhaseVoltage(PWMC_Handle_t *pHandle, alphabeta_t Valfa_beta)
pHandle->lowDuty = (uint16_t)wTimePhA;
pHandle->midDuty = (uint16_t)wTimePhB;
pHandle->highDuty = (uint16_t)wTimePhC;
pHandle->CntPhA = (uint16_t)(MAX(wTimePhA, 0));
pHandle->CntPhB = (uint16_t)(MAX(wTimePhB, 0));
pHandle->CntPhC = (uint16_t)(MAX(wTimePhC, 0));
uint16_t CntPhA; /**< PWM Duty cycle for phase A. */
uint16_t CntPhB; /**< PWM Duty cycle for phase B. */
uint16_t CntPhC; /**< PWM Duty cycle for phase C. */The function is called in FOC routine.
2023-12-21 11:03 PM
Thanks for your help.
I will try to test it.
2023-12-25 6:05 PM
@SRedd.5 Hi Sir, really thank you for your suggestion and I also found it in my mcsdk 5.4.5. Unfortunately, I'm able to call the variable to my main.c file. I want to see that CntPhA value as a live watch parameter in the IDE. May I know how can I call it? sorry for my poor programming skills.
2023-12-25 7:45 PM
To watch a variable live while the code is running two options are available
1. Enable a DAC channel and observe it on the scope.
2. Use Cube monitor tool using the ST link.
The option 2 is easy try it, you are not required to call the variable in the main.c file.
https://www.st.com/en/development-tools/stm32cubemonitor.html
2024-04-20 1:03 PM
Hi mate, i want max duty is 60%, because after rectifier AC220v i will get 310v dc but my motor only 200v, so if i used max pwm 60% iwill get avarage 186v right, how to se?? On that funtion stetphasa voltage?? Or change pulse value???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.