2018-09-07 12:12 AM
MCSDK has options only for PMSM. I would like to know whether MCSDK can also be used to control 3-Phase ACIM. If so, any details on the changes required will be helpful.
Thanks,
Prakash
Solved! Go to Solution.
2021-06-28 5:38 AM
Dear @PKris
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2018-09-07 7:46 AM
Dear Prakash,
Sorry but 3-Phase ACIM has not yet been implemented.
Thanks and best regards,
Claire
2021-06-27 10:27 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-28 5:38 AM
Dear @PKris
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-06-28 6:38 AM
Hi @Laurent Ca...
Thanks for the information. I'll definitely take a look at it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.