STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Custom board issue with STSPIN32G4

Hi.I am currently working on a custom board using the stspin32g4. This was derived from the evspin32g4 development board alone with the stm32 motor workbench. Uploading the motor workbench code to the evspin32g4, works and can tune the motor paramete...

jimmydvr_0-1744798321525.png
jimmydvr by Associate II
  • 1394 Views
  • 2 replies
  • 0 kudos

Resolved! Step motor control and max torque

Hello. I am doing stepper motor step control. I am using the "HAL_TIM_PWM_PulseFinishedCallback" function for this operation. Is there a more functional usage method than this? I can't get the max torque of the motor. Can you help me? Motor Driver "T...

AI_I by Associate III
  • 11146 Views
  • 14 replies
  • 1 kudos

Speed Feedback error

Hello,I am currently working with a custom board using an STGIB15CH60TS-LZ driver and an STM32H503RBT6 microcontroller.The motor is a 48V, 500W, 300 RPM brushless motor with three Hall effect sensors (120° mechanical angle, 300° electrical angle). It...

GetAttachmentThumbnail.jpg
Cedd by Associate II
  • 1329 Views
  • 1 replies
  • 0 kudos

Communication

Hello, I'm working with the ST EVAL3201 motor controller board. I'd like to use an STM32 Discovery board to send commands to start and stop the motor. Is this feasible? If so, could you provide guidance on the necessary connections and communication ...

AnilAJ by Associate
  • 1107 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to start motor with MC sdk generated code

hi, I have been trying to run PMSM motors with B-G431B-ESC1, I follow the steps given in the user manual, 1. I profile the motor and save the parameters 2. use the motor control workbench to generate a project, and generate source code, 3. run it in ...

madhavP by Associate II
  • 1221 Views
  • 1 replies
  • 0 kudos

Resolved! MCSDK 6.3.2 connectAlgo.log file not found

Hello,I got a error message during control project genaration"It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory feat...

STSPIN32G4 can't work with external 3.3V

Dear Community,////  For new members joining the discussion, please refer to our second reply, where we’ve shared more details about the modifications and testing done on our board.Thank you in advance for your interest and support!I’m currently deve...

Sheng123_0-1743954957852.png
Sheng123 by Associate II
  • 2076 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.