STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! MotorControl Workbench Issues

I have multiple issues to report with the MC Workbench (MCWB). I am using Version 6.3.2 and trying to get a dual motor BLDC setup working on custom hardware.In the .zip-file there is a minimal project required for viewing the issues and additionally ...

M_Schmidt by Associate III
  • 4040 Views
  • 5 replies
  • 3 kudos

Resolved! Current reading problem in 6.4.0

[PN]: Custom Board[VERSION]: 6.4.0 [TOOL]: MC WB[DETAILS]: I am using a custom board with a single shunt current sensing topology. However, in the Motor Control Workbench (MC WB), I cannot enable the "Current Reading" configuration option. I have see...

TKara2_0-1748382521520.png
TKara.2 by Associate III
  • 1258 Views
  • 2 replies
  • 0 kudos

Random Speed feedback errors

Hello,I am trying to control the speed of a PMSM with hall sensors. We are getting many random speed feedback errors that causes the drive to stop.When I looked at the code (hall_speed_pos_fdbk.c), I was surprised to find that the parameter bMaximumS...

Generate Code with Dual Motor on MC WorkBench

Hi ,We are working on NUCLEO- F401RE board for motor control and to configure & generate code MC WorkBench(version 6.3.2) is used. We have driven single motor, but we are not able to configure for dual motor below pop up appeared:Hardware Setup:Motor...

Harsh_M_0-1748002626853.png Harsh_M_1-1748002840722.png Harsh_M_2-1748002868874.png Harsh_M_3-1748002889583.png
Harsh_M by Associate II
  • 1560 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.