STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

3 phase BLDCdrivers

i am new to this BLDC motors and i am planning to build a 3-phase motor driver. attached the motor datasheet as well.Can anyone suggest a suitable driver for proof of concept for the attached motor specs.Link: https://www.maxongroup.com/medias/sys_ma...

Resolved! Can I select some other ST MCU in STMC board designer?

Hello Everybody,I'm designing a motor control board using the STM32F405 MCU in an LQFP64 package. When using STMC board designer, I noticed only a limited selection of MCUs is available (please refer to the attached picture ).  Could you advise how t...

bd_design_mcusel.jpg
DF_MC by Associate III
  • 1027 Views
  • 3 replies
  • 0 kudos

Resolved! HSO PolPulse Tune

hi,Question 1: Should I tune PolPulse directly at the end of profile? Without any pre-operation, such as changing "FOC Mode" from "profiling" to another one?Question 2: Which phases are the PWM waves and currents from? Are there any requirements when...

ZHOUXIANG_0-1755762209211.png ZHOUXIANG_1-1755762621258.png ZHOUXIANG_2-1755763555917.png
ZHOUXIANG by Associate III
  • 968 Views
  • 1 replies
  • 2 kudos

Motor Profiler with STEVAL-IPM30B power board

Hello, I wanted to make auto-tune for my engine but there is no STEVAL-IPM30B power board in Motor Profiler tool. Only IPM-05, 10, and 15 are supported. Can I select IPM-15B board and run Motor Profiler with a physically connected IPM-30B?

DJusz.1 by Associate II
  • 1606 Views
  • 3 replies
  • 0 kudos

Resolved! could't find X-CUBE-MCSDK on STM32cubeMX

hello i am making a custom STM32F405RGT6 board for A DUAL_BLDC_FOC VESC project that am making. i looked up how to programme the chip and it seems i needed to generate the code using STM32cubeMX  after instaling the X-CUBE-MCSDK embeded software pack...

rayboum_0-1755795090095.png rayboum_1-1755795228683.png
rayboum by Associate III
  • 1047 Views
  • 2 replies
  • 0 kudos

Resolved! Bus voltage acquisition

Hello everybody, I would like to know when the VBUS voltage measurement is updated. I am using the functions to read the voltage:VBS_GetBusVoltage_dVBS_GetAvBusVoltage_VI am using the threads startMediumFrequencyTask, StartSafetyTask, and my own thre...

Cedd by Associate II
  • 935 Views
  • 4 replies
  • 1 kudos

No such file or directory

Hi Team,I have created folder for header file and it's path also included in the compiler path but it's grayed out.but I'm getting this error.Could you help me on this one.

VINODC_0-1755779943683.png VINODC_0-1755779720801.png
VINODC by Associate II
  • 401 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.