STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Stm32 workbench issue

Me and my team have been working for a while now on the Stm32 workbench. The Motor Profiler calculates the parameters for the motor, and are then they are imported to the workbench to generate code to TrueStudio IDE. We are facing some issues with dr...

OTcho.1 by Associate
  • 2507 Views
  • 4 replies
  • 0 kudos

6-step examples from MC WorkBench not working

I tried two 6-step drive examples that come with MC WorkBench and could not make either of them to run a motor. First, I tried "Six-Step drive with NUCLEO-G431RB, IHM08M1 and Shinano motor". I did not have Shinano motor. A motor I have is very simila...

0693W000004GLWpQAO.png
ALabu.1 by Associate
  • 1984 Views
  • 3 replies
  • 0 kudos

Custom board MCU shorted and sensed voltage too low.

I am having trobule getting a custom motor control board to work. The design of the custom board is really close to the STEVAL SPIN 3201. So it uses the STSPIN32F0 and is supplied with 24V.When I start the motor and ramp up to the point where the bo...

MEmmo.1 by Associate II
  • 2121 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.