STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Low Speed Hall Sensor

Hi,I have been struggling to run my motor at low speeds and I suspect the Hall Sensors are the limiting factor. In UM1052 I found the following line on page 36. "For speed regulation, there is absolutely no need to have a sampling time lower than the...

nmamore by Associate II
  • 1981 Views
  • 1 replies
  • 0 kudos

Can a single STM32G4 be used to (sinusoidally) control 6 high-current BLDC motors, each with 3 digital Hall effect sensors, and each using 3x PWM Mode for control?

We would like to use an STM32G4 to (sinusoidally) control 6 high-current BLDC motors, each with 3 digital Hall effect sensors, and each using 3x PWM Mode for control (in addition to monitoring the voltage across 1 or 3 shunt resistors on each motor f...

Ricardo1 by Associate II
  • 1313 Views
  • 1 replies
  • 0 kudos

B-G431B-ESC1 batch B04 issues

I've got 2 units of B-G431B-ESC1 version Y batch B04 and been struggling for 2 weeks already. Tried all the hacks on https://community.st.com/s/question/0D53W00000HwV8RSAV but they are still not working properly. The latest and best tried so far was ...

PPhan.1 by Associate II
  • 1614 Views
  • 2 replies
  • 0 kudos

Resolved! B-G431B-ESC1 from Batch B04 not working

I've tried numerous boards, with different motors and power supplies.I just can't seem to get it to work, neither using motor profiler or motor control workbench (using the example code).After reaching out to some other people that had the same probl...

EGran.2 by Associate II
  • 3261 Views
  • 6 replies
  • 0 kudos

How drive a motor using modbus and stm32f103 controller

Hi,I am doing project on stepper motor using stm32f103 controller and I need to drive my motor using modbus.So i need to calculate acceleration , deacceleration and speed, distance and time and frequency of my motor using trapezoidal motion profile ....

Lchal.1 by Associate III
  • 1417 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.