STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Problem with FOC Lib 4.0 examples

Posted on June 25, 2015 at 09:14I started to learn to use FOC Lib 4.0 to control a PMSM motor with encoder. I used MC workbench to configure the HW and generated code to SystemDriveParams, then I used the example project for STM32F30x_Workspace.uvmp...

song by Associate II
  • 1706 Views
  • 2 replies
  • 0 kudos

Motor Control Workbench 4.1

Posted on August 17, 2015 at 15:00Hi, I’m using the state observer + PLL algorithm and observer + CORDIC and i try to figure out the GAIN1, GAIN2, scaling factors and PLL KP / KI how the coefficients are calculated by ST MC Workbench v4.1 thanks fo...

Workbench limitations

Posted on August 26, 2015 at 09:19Hi, i want to run motors with Rs < 0.01 Ohm and Ld<0.010 mH (low voltage high current), but the Motor Control Workbench is limited to this values. Can someone give me the formula to compute all the parameters from t...

ST MC workbench Current sense

Posted on September 24, 2015 at 19:54Hi,I am using ST MC Workbench to design a BLDC FOC motor driver, and am running into a problem.  I am using three shunt resistors to sense current (one per channel) and am trying to use ''embedded PGA'' as an amp...

STM Studio - STM32 PMSM FOC LIBv4.2 variables

Posted on October 14, 2015 at 23:54Hi, I am running the STM32 PMSM FOC LIBv4.2, using encoder and I am trying to visualize the variables values through the STM Studio. The variable names used here are the default used in the STM32 PMSM FOC LIBv4.2I ...

cviolino by Associate II
  • 1258 Views
  • 2 replies
  • 0 kudos

ST Motor Control Workbench Under Voltage Fault

Posted on February 18, 2016 at 20:17I'm using the ST Motor Control Workbench with STEVAL-IFN003V1 and my bus voltage is reading above the threshold but the Under Voltage fault light is constantly on even if I disable the low voltage checking in the ...

Konami by Senior II
  • 1517 Views
  • 2 replies
  • 0 kudos

STM3240G recommended Motor kit IHM-???

Posted on March 31, 2016 at 22:03Hi, I am not having much luck with the Nucleo-IHM001 eval kit(s), for now going to put them down, very dissapointing. I have a STM3240G eval board that appears to be supported by the ST motor control workbench. Can a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.