STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Connecting EVSPIN32f0601S1 to Motor Pilot

Hi, I'm new to the STMicroelectronics environment and I'm having issues with the EVSPIN32F0601S1 development board. I'm trying to spin a motor but I'm having issues connecting the evaluation board to the Motor Pilot GUI. I followed the video from the...

0693W00000NsjJ3QAJ.png 0693W00000NsjIoQAJ.png 0693W00000NsjItQAJ.png 0693W00000NsjIyQAJ.png
KMarc.1 by Associate
  • 1673 Views
  • 1 replies
  • 0 kudos

Resolved! stm32g4xx_mc_it.c and stm32g4xx_it.c

Hi, I am using CubeMX generates the application that contains MCSDK, The generated code has both stmg4xx_mc_it.c and stm32g4xx_it.c. I noticed that all the motor control related ISR code are coded in stm32g4xx_mc_it.c and I am confused with 2 issues:...

YWang.15 by Associate II
  • 1689 Views
  • 1 replies
  • 0 kudos

Generate or create a .ioc for induction motor

After getting the example ACIM program running (Nucleo-G431RB and STEVAL-IHM023V3), I want to customize beyond those two boards. To do this, I believe I need to generate (or hand-make) a .ioc file.Trying to generate a file through MC WorkBench just ...

Dane._.T by Associate II
  • 993 Views
  • 0 replies
  • 0 kudos

Resolved! (5.Y.4) Errors since upgrade to 5.Y.4 when building project with Cube IDE (and error "ST Intranet updater server unknown" in Workbench code generation)

Hello, I recently moved to the new 5.Y.4 version of the SDK because I am using a custom PCB based on STSPIN32G4 with external OPAMP resistor network (external gain) and after hours of searching I found out that 5.Y.3 doesnt support OPAMP in standalon...

0693W00000NsoRMQAZ.png 0693W00000NsoQxQAJ.png
ALedi.1 by Associate III
  • 2845 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.