STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

How to run a small induction motor with STEVAL-CTM012V1

I am trying to run a small, three phase induction motor from a single phase supply. The STEVAL-CTM012V1 has more than enough power rating. I have wasted hours trying to get something working. All the files I can download seem to want to do fancy FOC ...

Dense505 by Associate II
  • 1442 Views
  • 1 replies
  • 0 kudos

STSPIN32G4 buck output dropped trigger uvlo protection

I use Internal comparator trigger Timer etr function to impelement cycle-by-cycle current mode control. I got uvlo protection when motor at heavy load(~40A pk).But when i use voltage control ,it would not occur. Does any one occur this problem?​GHSU-...

0693W00000WJaakQAD.jpg 0693W00000WJaaaQAD.jpg 0693W00000WJaaLQAT.jpg
XShiy.1 by Associate
  • 872 Views
  • 0 replies
  • 0 kudos

How to control Stepper Motor with Nucleo-L476RG

I am using the Nucleo-L476RG and I have bought a 28byj-48 Stepper motor with the ULN2003 Driver. I need to control the motor using STM32CubeIDE and am wondering how to configure a stm project to control the motor at any capacity.

JEscu.2 by Associate II
  • 2287 Views
  • 1 replies
  • 0 kudos

stm32f334 llc full bridge

hi any one can help how to got sorce code stm32f334 for full bridge i need for design 10kw sic dc to dc this power not allowing on online desin st

FOC command is sometimes stuck

Hello, I'm controlling a BLDC motor with MCSDK 6.0.0 and IHM08M1, with FOC with 1024 PPR encoder. I compute torque (Iq_ref) commands to achieve speed control, this works ok except in rare case described below:Sometimes the MCSDK seems "stalled": I se...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.