STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Porting from B-G431B-ESC1 to custom board

Hello all,I have a 20 pole pair, 100v, 120Amp, 15mOhm. 34uH,  sensorless, BLDC outrunner motor.I have had this running on the B-G431B-ESC1 dev board with 25v at 800 RPM drawing 1.5 Amps. The power supply being lab bench supply capably of 30vDC and 5A...

B-G431B-ESC1 Motor Profiler "Over Voltage"

I'm using ST Motor Pilot V1.1.5 with eval board B-G431B-ESC1.Motor: IBL-100SW-1 http://www.itomotor.com/product/detail/67.htmlMotor Profiler Configuration:Pole Pairs: 3Max Speed: 2000 RPMMax peak current: 5 AMagnetic: I-PMSMld/Lq: 1After starting the...

Marc1 by Associate III
  • 2294 Views
  • 3 replies
  • 0 kudos

B-G431B-ESC1 over current fault after setup.

I was able to run the ST MC Workbench toolfor motor and parameter configuration successfully and the motor ran fine. I then uploaded the generated code through STM32CubeIDE however once uploaded when I try to start the motor there is an audible click...

MMcLe.2 by Associate
  • 2927 Views
  • 3 replies
  • 2 kudos

Resolved! STEVAL-PTOOL2V1

I am trying to work with the STEVAL Ptool2v1 BLDC controller, but have had no success in getting it to work. I have downloaded the STSW-PTOOL2V1 software and unbundled it to a hierarchal dir system, which leads to a project dir, where there is a proj...

DDoug.2 by Associate
  • 1369 Views
  • 1 replies
  • 0 kudos

How do I flash firmware to the B-G431B-ESC1?

I'm trying to get the basic firmware running, but I think I'm doing something wrong because the ESC doesn't seem to function. I've generated an IDE project for the B-G431B-ESC1 using the ST Motor Control Workbench, which I then opened in STM32CubeIDE...

ZRoma.1 by Associate
  • 4111 Views
  • 1 replies
  • 0 kudos

MCSDK 5.4.8 g++ compile problem

I don't know where to report it. In the file MotorControl/MCSDK/MCLib/Any/Inc/hall_speed_pos_fdbk.hIn Line 232 is missing:...#ifdef __cplusplus}#endif /* __cpluplus */....#endif /*__HALL_SPEEDNPOSFDBK_H*/

JRyba.2 by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

Resolved! need a 5kW motor driver board

Hi all,       I'm Siva, and i need a BLDC motor driver to run a 5kW motor. please suggest me in buying out the right driver board. the voltage needed for the motor is 48 volt and the current needed will be 180A.   

Resolved! Motor not working as expected

I'm trying to make run a motor via Motor Pilot but it does not work correctly. I'm using the following motor: 1 stücke Mitoot 5008 335KV/400KV Bürstenlosen Motor Für 1555 1755 Propeller Quad kit RC Multicopter Hexacopter Tarot T960 t810|Teile & Zubeh...

GJamo1_1-1687706903988.png GJamo1_0-1687706565796.png
GJamo.1 by Associate II
  • 1656 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.