STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Flux Weakening Torque Control Mode

I want to use the flux weakening in my project using Workbench 6.2 i generated the code using the below settingwhen i select the speed control mode i can see the tab to select the Flux Weakening regulator.But when i select the torque control mode The...

SRedd5_0-1697259954346.png SRedd5_1-1697260044035.png
SRedd.5 by Senior III
  • 2732 Views
  • 1 replies
  • 1 kudos

Resolved! MC SDK v6.2.0

Hello,I am trying to use the MC SDK v6.2.0 for controlling a PMSM and I wish to control the motor through my host PC with uart protocolI have got below document which is for SDK v4.3.Can you please share similar user manual for SDK v6.2.0Can you also...

X-NUCLEO-IHM12A1 - STSPIN240 DC MOTOR DRIVER

Hi,We used X-NUCLEO-IHM12A1 to run a single DC Motor which was connected to A+ and A- pins.The Vref voltage for the motor driver can be set to maximum of 0.5V as per the datasheet. The motor stall current  for our motor as per the datasheet is 370mA....

NIVI by Associate III
  • 1241 Views
  • 1 replies
  • 0 kudos

Resolved! Cordic Function in L series of STM32

We started using the L series of the ST Micro for a project and found that it does not have CORDIC functions. What is the best way forward? Do we need to implement on our own? Or we have to migrate to G4 series. 

SRedd.5 by Senior III
  • 3084 Views
  • 4 replies
  • 3 kudos

MCSDK 6.2 and IHM042-V1 Dual Motor Position Control

Version:  MCSDK 5.4.8 / MCSDK 6.2.0Tool: Firmware / MC WBEvaluation Board: IHM042-V1Details:When using MCSDK 5.4.8 I am unable to have the first motor perform in the same manner as the 2nd motor despite all parameters being identical and the same mot...

95Z_0-1696419881195.png
95Z by Associate
  • 1793 Views
  • 2 replies
  • 0 kudos

Resolved! Some confusion about MCSDK 6.2.0

[VERSION]: 6.2.0[TOOL]: ST Motor Pilot/ MotorControl Workbench 6.2.0[DETAILS]:1.The speed ki ‘s numerical values ​​do not correspond.It is different from 5.Y.4.2. About the Board Maneger. I want to add my own board but no documentation guidance.3. Ab...

企业微信截图_16968470027075.png
gtop.1 by Associate III
  • 3336 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.